DOCA0265EN-07

Opening Function

Presentation

MicroLogic Active control units receive and process electrical opening orders. An event is generated on opening.

Operating Principle

Opening orders can be sent as follows:

  • Directly through a mechanical opening pushbutton.

  • Locally through an external opening pushbutton, connected directly or via the BCIM module to the MX communicating opening voltage release

  • Remotely through a remote order which is managed by the MicroLogic Active control unit.

Opening orders have priority over closing orders. No closing orders are taken into account as long as an open order is active.

The open orders on MN or MX voltage releases by external pushbutton can be maintained to force the circuit breaker in open position and reject any close order. The MicroLogic Active open orders are not maintained.

Management of Opening Function

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
  • Do not operate the circuit breaker without confirming that doing so will not create a hazardous situation.
  • Do not use MicroLogic Active remote control functions in a safety chain.
  • Do not allow any person to work on the electrical network without physically validating the successful execution of the local or remote software actions for opening the circuit breaker or switching off the electrical circuit.
Failure to follow these instructions will result in death or serious injury.

The MicroLogic Active control unit manages opening orders issued by the following means:

The control logic for managing opening orders is summarized in the following graphic and table:

CB closed

Circuit breaker is closed

Auto Local

Control mode is Auto Local

MX control by BCIM enabled

Control of the MX voltage release by the BCIM module is enabled.

BCIM IO mode=Open/Close

The BCIM IO mode parameter is set to Open/Close.

BCIM IO open

Open order from the opening pushbutton connected to the BCIM module

FDM121 open

Open order from FDM121 display

Auto Remote

Control mode is Auto Remote

COM open

Open order from a server or remote controller

Webpage open

Open order from IFE/EIFE webpage

Open

MicroLogic Active open order to the MX communicating opening voltage release

Predefined Events

The function generates the following predefined events:

Code

Event

History

Severity

0x1000 (4096)

Circuit breaker opened

Operation

Low

0x0410 (1040)

Opening order sent to MX voltage release

Operation

Low

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.