DOCA0265EN-07

Management of Access via the USB Port

Description

Access to data via the USB port is done with:

Access via the USB port is protected by the USB password. This password has no expiry date.

USB Password Creation

When you connect to EcoStruxure Power Commission software or EcoStruxure Power Device app, you are prompted to create a SecurityAdmin account. You can postpone account creation by selecting Skip.

The default password is schneider123.

USB Password Change

The USB password can be changed with EcoStruxure Power Commission software.

Entering the current password is required to change the password.

A password is composed of 8 to 32 ASCII characters, with the following constraints:

  • Only ASCII [32–126] allowed

  • At least one uppercase character

  • At least one lowercase character

  • Must not contain the username

  • Must be different to the previous password

USB Password Reset

The USB password can be reset by pressing Reset Password when connecting to EcoStruxure Power Commission software or EcoStruxure Power Device app.

After pressing Reset Password, a confirmation pop-up message appears on the screen. Click to confirm and complete the procedure.

NOTE: reset of the USB password also results in reset of the PIN code.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.