DOCA0265EN-07

Management of Access via HMI

Description

Access to MicroLogic Active data is available on the MicroLogic Active HMI.

Access to protected parameters is protected by a PIN code. This PIN code has no expiry date.

By default, the PIN code is associated with the SecurityAdmin account.

When you access a protected parameter for the first time, you are prompted to create a SecurityAdmin account and set a PIN code. You are then prompted to enter the PIN code each time you access a protected parameter. If you enter the wrong PIN code 5 times, the account is locked for 4 minutes.

You can postpone account creation by selecting Do it later. In this case, you are prompted to create an account each time you access a protected parameter.

The following actions are protected by PIN code:

  • HMI PIN code modification

  • Protection function setting

  • Protection function testing

  • Date and time modification

  • Control mode modification

  • Replacement MicroLogic Active setting

PIN Code Change

The PIN code can be changed on the MicroLogic Active control unit HMI.

The PIN code must consist of 6 digits, from 0 to 9.

PIN Code Reset

The PIN code can be reset by pressing Reset all users when connecting to EcoStruxure Power Commission software or EcoStruxure Power Device app.

After pressing Reset all users, a confirmation pop-up message appears on the screen. Click to confirm and complete the procedure.

NOTE: reset of the USB password also results in reset of the PIN code.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.