MEG6194-6010S_SW_24_06_14

Application Examples for Edge Function

The following activation sequence chart shows the phases into which the edge function is divided.

Extended edge function sequence chart

Normal edge function sequence chart

Operate button
Release button
Object A Sends telegrams
Sends 1/None Action on operation/action on release

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?