MEG6194-6010S_SW_24_06_14

Staircase Lighting Function with Cleaning Light Function

With a brief button action, the switch actuator switches on the light. A long button action extends the staircase lighting function (= cleaning light function) until a second, long button action switches off the actuator. The switch actuator requires a staircase lighting function and a locking function for this function.

  • Number of objects = 2 (object A/B)

  • Object A/B = 1 bit

  • Object A:

    • Action on release before the long operating time has elapsed = Sends 1

    • Other actions = None (stops cyclical sending)

  • Object B:

    • Action on achieving the long operating time = Toggles.

    • Other actions = None (stops cyclical sending)

To do this, connect object A to the Switch object and object B to the Locking object of the switch actuator.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?