MEG6194-6010S_SW_24_06_14

Cleaning Mode

You can set the time to exit cleaning mode after you turn it on.

Press and hold one button on each side of the panel for 10 seconds at the same time to trigger the countdown.

The countdown displays on the screen. All buttons are temporarily disabled during the countdown.

The device turns on automatically after the time you set (5 s – 60 s).

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?