MEG6194-6010S_SW_24_06_14

Device Type

Depending on the product type, the product diagram displays here.

For the 1/2/3-gang type, you can not change the number of buttons on the right and left. The universal type allows you to select the number of left and right buttons from 1 to 4.

General settings

Device type

 

Device type

Universal/1-gang/2-gang/3-gang

   

Device setting for

Left side/Right side

   

Number of buttons

1 – 4

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?