Two-Button Operation for Blind
You can now move the blind either up or down by pressing and holding the corresponding button. A short button action stops the travel. A short button action also adjusts the slats in steps. You can set the operating time for the long button action.
|
Function X – Blind ...Blind |
Extended settings for blind |
||
|
Movement direction of blind |
Moving up or Moving down |
||
|
Time for long operation |
4 – 250, unit = 100 ms |
The blind is moved up or down via the Movement object, while the stopping and adjusting of the slats is controlled via the Stop/step object. You need 2 button functions, each of which you connect to the same group addresses.