Display Settings
In the Display settings section, you can set the display backlight level in normal, night, and standby mode.
|
Extended settings |
Display settings |
||
|
Backlight level in normal mode |
5 – 100 % |
||
|
Backlight level in night mode |
5 – 100 % |
||
|
Standby mode |
Tick/Untick |
||
|
Temperature display units |
Celsius/Fahrenheit |
It is possible to set the units for displaying the temperature. This setting affects all the temperature displays, including the middle field and the screen saver temperature.
If you allow standby mode, you can also customize the appearance of the standby display.
The device switches back to normal mode via the proximity sensor or buttons.
If you choose Date and time interface and enable the proximity function you can use this parameter to set when your interface automatically returns to normal mode when waking up. If you choose Temperature or Date, time, and temperature, you can select which temperature you want to display on the standby screen (internal/external/both).
If the user does not operate the device within the preset time, the device switches from normal to standby mode. The time interval can be influenced by the proximity Off delay parameter.
The device awakes first to standby and then enters normal mode either with preset delay or if you press any button. If you disable the proximity function and select Unchange for standby display, you have to press any button to return from standby to normal mode.
See more in Proximity Function.
You can choose to display the temperature from internal, external, or both sensors and name them.