Object Type
You can send the values via the following objects to the bus by pressing a button:
|
Object type |
Adjustment options |
Devices |
|---|---|---|
|
Temperature setpoint (DPT 9.001) |
Temperature setpoint |
MTN6730-0002 or most of the temperature control panels. |
|
Absolute setpoint value |
||
|
Relative setpoint value |
||
|
Temperature shift (DPT 9.002) |
Reference temperature difference 2 bytes |
MTN6215-5910 MTN6730-0003 |
|
Temperature shift (DPT 6.010) |
Reference temperature difference 1 byte |
MTN6730-0002 |
To display the temperature setpoint value in the middle field, you need to set the Setpoint input of the middle field display in the same group with temperature setting object of the valve.