Start-up and Test
Before using electrical control and automation equipment for regular operation after installation, the system should be given a start-up test by qualified personnel to verify correct operation of the equipment. It is important that arrangements for such a check are made and that enough time is allowed to perform complete and satisfactory testing.
WARNING |
|---|
|
EQUIPMENT OPERATION HAZARD
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
Follow all start-up tests recommended in the equipment documentation. Store all equipment documentation for future references.
Software testing must be done in both simulated and real environments.
Verify that the completed system is free from all short circuits and temporary grounds that are not installed according to local regulations (according to the National Electrical Code in the U.S.A, for instance). If high-potential voltage testing is necessary, follow recommendations in equipment documentation to prevent accidental equipment damage.
Before energizing equipment:
-
Remove tools, meters, and debris from equipment.
-
Close the equipment enclosure door.
-
Remove all temporary grounds from incoming power lines.
-
Perform all start-up tests recommended by the manufacturer.
WARNING