MEG6194-6010S_SW_24_06_14

Temperature Decrease/Increase

The Temperature decrease function allows you to change the temperature setpoint value. When you assign this function to the button and press it, the setpoint temperature displays in the middle field if you select Temperature only or Temperature + text in General settings (Middle Field Display).

The Temperature increase function is the same as the Temperature decrease function. The only difference is that it is used for increasing the setpoint temperature value.

You can change the following settings:

Function X – Temperature decrease/increase

Temperature decrease/increase

Settings for temperature decrease/increase

Name of the channel

12 bytes allowed

Locking function

Disable

Locking = 1/Unlocking = 0

Locking = 0/Unlocking = 1

   

Behavior indication when locking

No

Display lock icon

   

Object type

Temperature setpoint (DPT 9.001)

Temperature shift (DPT 9.002)

Temperature shift (DPT 6.010)

   

Temperature adjust step

0,1 – 0,5 K

 

[Temperature decrease]

Minimum setpoint

10 – 32, unit = 1°C

 

[Temperature decrease]

Minimum setpoint shift

– 0, unit = 1 K

 

[Temperature increase]

Maximum setpoint

10 – 32, unit = 1 °C

 

[Temperature increase]

Maximum setpoint shift

0 – 10, unit = 1 K

   

How the status indication is triggered

Status feedback object 1 bit

Status feedback object value 1 byte

Operation = On/Release = Off

Operation = Off/Release = On

Always on = Off

Always on = On

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?