Single-Button Operation for Blind
A long button action alternately raises or lowers the blind. The current movement direction of the blind is always dependent on the previous action. You can set the operating time for the long button action.
You can adjust the slats in the same direction in multiple steps. To do so, briefly press the button repeatedly until the desired position is reached. The slats adjust in the same direction provided that the next button action follows within an adjustable pause time. Once this pause elapses, the slat direction of rotation changes.
|
Function X – Blind ...Blind |
Extended settings for blind |
||
|
Movement direction of blind |
Moving up/down |
||
|
Pause for change slat direction |
5 – 50, unit = 100 ms |
||
|
Time for long operation |
4 – 250, unit = 100 ms |
The blind is moved alternately up and down via the Movement object, while the stopping and adjusting of the slats is controlled via the Stop/step object.