MEG6194-6010S_SW_24_06_14

General Settings

In the General settings section, you can select the functions and the number of buttons on the left and right. You can assign specific functions to the buttons and select icons for the middle display.

Long and short operations are preset:

  • For a short operation, press < 0,5 s.

  • For a long operation, press ≥ 0,5 s.

  • To save a scene, press ≥ 10 s.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?