MEG6194-6010S_SW_24_06_14

Restoring Defaults

You can set the factory-specified defaults using the Default parameters service button in the ETS.

You can use the Default and Default parameters service buttons to switch all parameters back to the settings on delivery (following consultation). The ETS will then permanently delete all manual settings.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?