MEG6194-6010S_SW_24_06_14

RGB Lighting

The RGB lighting function allows you to set a specific RGB or RGBW LED color. In ETS, you set the RGB/W value and connect it to a specific button.

The user calls up the set lighting color by pressing the button.

You can change the following settings:

  • Type of object value

  • Distinction between long and short operation

  • RGB/W value

  • Tunable white color temperature control

Function X – RGB lighting

...RGB lighting

Settings for RGB lighting

 

Name of the channel

12 bytes allowed

Locking function

Disable

Locking = 1/Unlocking = 0

Locking = 0/Unlocking = 1

   

Behavior indication when locking

No

Display lock icon

   

RGB strip type

RGB

RGBW

   

Object type

1 × 3 byte

3 × 1 byte

1 × 6 byte

4 × 1 byte

   

Number of operations

1 (short operation)

2 (short/long operation)

   

Time for long operation

4 – 250, unit = 100 ms

   

Send value (short operation)

 
   

RGB value 1

 
   

White value 1

 
   

Send value (long operation)

 
   

RGB value 1

 
   

White value 1

 
   

How the status indication is triggered

Status feedback object 1 bit

Status feedback object value 1 byte

Operation = On/Release = Off

Operation = Off/Release = On

Long operation = On/Release = Off

Always on = Off

Always on = On

You can dim each color with separate bytes or you can dim all colors together through one group object.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?