MEG6194-6010S_SW_24_06_14

Normal Scene Function

A short button action calls up a scene. A long button action saves the current values for the scene.

Function X – Scene

...Scene

Express settings for scene

 

Name of the channel

12 bytes allowed

Locking function

Disable

Locking = 1/Unlocking = 0

Locking = 0/Unlocking = 1

   

Behavior indication when locking

No

Display lock icon

   

Scene address

0 – 63

   

How the status indication is triggered

Status feedback object 1 bit

Status feedback object value 1 byte

Operation = On/Release = Off

Operation = Off/Release = On

Long operation = On/Release = Off

Always on = Off

Always on = On

   

Extended settings for scene

 

Call up room functions

You can use a scene to change multiple room functions at the touch of a button.

Loading a scene allows you, for example, to dim the room lighting to a specific value, move the blinds into the desired position and switch on the power supply to the socket-outlets in a room.

Save room functions

You can change the values for the individual room functions in a scene. To do this, use further button functions such as switching, dimming or move blind. You can use these button functions to change the values for the room functions consecutively. You then save the new values to the scene button by pressing and holding the button.

Settings

In the normal scene function, the parameter Scene address (0 – 63) appears. You can use this value to call up a scene in actuators and in scene modules. The values for saving are assigned automatically. You can adjust the duration of a long button action. The default setting is a duration of 600 ms.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?