MEG6194-6010S_SW_24_06_14

Status Indication

In the default setting, the status indication is triggered by the Switch/value object = On/Off.

Trigger

Note

Switch/value object A/B = On/Off

If the object is 1 byte, the value > 0 = the state is On, and the value 0 = Off.

Status feedback object 1 bit

1 = On

0 = Off

according to the value of the 1-bit external feedback object.

Status feedback object 1 byte

If the feedback value of the external object is 1 byte,

the value > 0 = On,

and the value 0 = Off.

Operation = On / Release = Off

The pressed button state = On

Release button state = Off

Operation = Off/Release = On: The pressed button state = Off, and the release button state = On.

Always on = Off/On:

The icon is always Off/On.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?