MEG6194-6010S_SW_24_06_14

Single-Button Dimming

In the default setting, a single command is sufficient to run through the dimming range. Hold the button down until the required level of brightness has been reached.

When you release the button, the Dimming object sends a stop telegram and ends the dimming process.

If desired, you can divide the dimming process into dimming steps (1/2 to 1/64 brighter or darker).

If you select 1/4 brighter, you can dim a maximum of 25 % brighter with each button action. The dimming process also ends in this case when you release the button.

You can send dimming commands cyclically. The dimming process ends when you release the button.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?