MEG6194-6010S_SW_24_06_14

Extended Settings for Dimming

Function X – Dimming

...Dimming

Extended settings for dimming

Enable

Time for long operation

4 – 250, unit = 100 ms

Dimming direction

Dimming brighter

Dimming darker

Dimming brighter/darker

 

Step dimming

1/2 to 1/64

   

Send stop telegram after release

 
 

Send dimming command cyclically

Enable

 

Basis

0,1 s

1 s

1 min

   

Factor

3 – 255

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?