MEG6194-6010S_SW_24_06_14

Dimming

With Dimming, you can switch and dim the dimmable lighting with 1 or 2 buttons.

Two-button dimming is the default setting. A short button action switches on or off. A long button action dims brighter or darker. Releasing after pushing and holding the button ends the dimming process.

You can change and extend the dimming function with the following functions:

  • Dim alternately brighter or darker with each button (single-button operation)

  • Only dim brighter or only darker with each button (two-button operation)

  • Operating time for long button action

  • Dim in steps with multiple dimming commands

  • Send dimming command cyclically

  • Trigger status indication

Function X – Dimming

...Dimming

Express settings for dimming

 

Name of the channel

12 bytes allowed

Locking function

Disable

Locking = 1/Unlocking = 0

Locking = 0/Unlocking = 1

   

Behavior indication when locking

No

Display lock icon

   

How the status indication is triggered

Switch/value object A = On/Off

Status feedback object 1 bit

Status feedback object value 1 byte

Operation = On/Release = Off

Operation = Off/Release = On

Long operation = On/Release = Off

Always on = Off

Always on = On

   

Extended settings for dimming

Enable

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?