MEG6194-6010S_SW_24_06_14

Locking Function

In the Express settings, you can name the channel and set the button lock.

The button is locked via the 1-bit Button locking object with values 1 (lock) and 0 (unlock).

You can reverse value sending: 0 (lock) and 1 (unlock). The locked button can be indicated by a lock icon or not at all.

If you select Disable, the locking function becomes inactive.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?