MEG6194-6010S_SW_24_06_14

Moving Blind with Positioning Values

If the blind actuator supports activation of positions, you can use this function to set 1 or 2 positions. You can select the positioning values to be absolute (0 – 255) or a percentage.

If positioning is activated, when you press the button, the set values for the blind position and slat position are sent.

If you have set 1 position, the values for the blind and slats are sent when you press the button briefly.

If you have set 2 positions, you specify a total of 4 values. You send the values for position 1 after a brief button action and the values for position 2 after a long button action.

Function X – Blind

...Blind

Extended settings for blind

 

Movement direction of blind

Moving with positioning values

Number of positionings

1 (short operation)

2 (short/long operation)

 

Type of position values

Moving blind with positioning values

   

Number of positionings

0 – 100%

0 – 255

   

Position 1/2 of blind

 
   

Position 1/2 of slats

 

You send the values for the positions via the 1-byte objects Blind position and Slat position.

The movement object and stop/step object are not available if you move the blinds with positioning values.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?