Normal Edge Function
With the normal edge function, you can specify which actions should be carried out when a button is pressed, and which should be carried out when a button is released.
You can set the following actions:
|
Value |
Action |
|---|---|
|
Sends value 1 |
Sends value 1 and stops cyclical sending. |
|
Sends value 2 |
Sends value 2 and stops cyclical sending. |
|
Sends its value |
The current object value is sent. Therefore you can, for example, send a value with the sending group address that was previously received via another group address. In so doing, you save a setpoint in the push-button and this value is sent when needed. |
|
None |
No action is carried out. |