8-Bit Slider
With the slider function, you can send values stepwise or cyclically with 1 button. The values are increased or reduced in steps.
You can operate the button in 2 ways:
-
Send a value with each button action (press 5 times to send 5 values).
-
Send values cyclically when pressing and holding the button.
If you want to send multiple values, press and hold the button until the last value is sent.
By default, the object value is raised by the value "10" if you release the button before the long operation time elapses.
You can select the following functions:
-
Slider with or without limit values
-
Step width of slider
-
Either increase or reduce values per button action
-
Either increase or reduce values until release
-
Either increase or reduce values cyclically from the starting value
-
First increase then reduce values per button action
-
Toggle direction and send values cyclically