MEG6194-6010S_SW_24_06_14

Color Temperature Control

With the Color temperature control function, you can send the preset percentage of brightness and the value of color temperature expressed in Kelvins (K).

You can select the minimum and the maximum color temperature values. The usable value range depends on the control device and the lamps. The control device has to support the 2-byte data point type 7.600.

Function X – Color temperature

... Color temperature

Settings for color temperature control

 

Name of the channel

12 bytes allowed

Locking function

Disable

Locking = 1/Unlocking = 0

Locking = 0/Unlocking = 1

   

Behavior indication when locking

No

Display lock icon

   

Number of operations

1 (short operation)

2 (short/long operation)

   

Time for long operation

4 – 250, unit = 100 ms

   

Send value (short operation)

 
   

Brightness value 1

 
   

Colour temperature value 1

 
   

How the status indication is triggered

Status feedback object 1 bit

Status feedback object value 1 byte

Operation = On/Release = Off

Operation = Off/Release = On

Always on = Off

Always on = On

With lighting, the color temperatures differ according to the type of source:

  • Candle light: 1500 K

  • Incandescent bulb: 2600 K – 2700 K

  • Halogen bulb: 2700 K – 3000 K

  • Fluorescent light: 4500 K – 6500 K

  • Daylight: 5500 K – 7000 K

The higher the number of Kelvin, the cooler white the light is. The lower the number of Kelvin is the warmer and more yellower the light is.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?