Status Indication
In the default setting, the status indication is triggered by pressing the button.
|
Trigger |
Note |
|---|---|
|
Switch/value object A = On/Off |
If the object is 1 byte, the value > 0 = the state is On, and the value 0 = Off. |
|
Switch/value object B = On/Off |
If the object is 1 byte, the value > 0 = the state is On, and the value 0 = Off. |
|
Status feedback object 1 bit |
1 = On 0 = Off according to the value of the 1-bit external feedback object. |
|
Status feedback object 1 byte |
If the feedback value of the external object is 1 byte, the value > 0 = On, and the value 0 = Off. |
|
Operation = On / Release = Off |
The pressed button state = On Release button state = Off Operation = Off/Release = On: The pressed button state = Off, and the release button state = On. |
|
Long operation = On / Release = Off |
The long operation state = On Release button state (or short operation) = Off |
|
Always on = Off/On: |
The icon is always Off/On. |