MEG6194-6010S_SW_24_06_14

Startup Delay

Startup delay is a time by which the device startup delays after power-on. The device initialization time is not included.

Set the value from 0 (disabled) – 30 seconds.

During the delay period the device sends no telegrams to the bus and the channels do not change their state.

After the delay expires, the telegrams are sent and the state of channels is set according to the parameters defined.

Any telegrams received from group objects during the delay period get stored. Replies to these telegrams are sent after expiry of the delay time.

You can use the startup delay to reduce load on the bus and supply circuit after power-on. It also informs you that the bus is ready for communication and the devices are powered.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?