Overview of Functions
The number of buttons and functions varies by module. The following overview refers to the universal module.
|
Button function |
Function 1 – 8 |
|
Device type |
Device type Device setting for the left and right side Number of buttons |
|
Connect button with function |
Button function – Left/Right side Button 1 – 8 |
|
Middle field display |
Indication type of line 1 – 4 |
|
Startup-delay |
Additional startup-delay of application |
|
Device health |
Cyclic sending live signal |
|
Night mode |
|
|
Cleaning mode |
Time setting for cleaning mode |
|
Interface language |
|
|
Display settings |
Backlight level in normal/night mode Standby mode |
|
Orientation indicator |
Indicator visibility Color and brightness of LED |
|
Proximity function |
How the proximity function is triggered Type of output object Send output value cyclically |
|
Internal temperature sensor |
Internal sensor compensation Datapoint type for temperature object Send temperature when the result changes by Cyclically send temperature |
|
Express/Settings for function 1 – 8 |
No function |
|
Icon configuration |
Toggle |
|
Switch |
|
|
Dimming |
|
|
Blind |
|
|
Edges 1-bit, 2-bit (priority), 4-bit, 1-byte |
|
|
Edges with 2-byte values |
|
|
8-bit slider |
|
|
Scene |
|
|
RGB lighting |
|
|
Color temperature control |
|
|
Temperature decrease |
|
|
Temperature increase |
|
|
Logic functions |
1st – 8th logic function |