MEG6194-6010S_SW_24_06_14

Behavior When Bus Voltage Is Connected/Recovered

Behavior when bus voltage is connected / recovered

Depending on the application settings, the status LEDs are switched on or off or they flash.

Behavior when bus voltage fails

Any status LEDs that were lit are switched off.

The current values of the group objects are not saved.

Configuration mode

After a download, the device goes into configuration mode for a few seconds. During this time, the LED flashes.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?