MEG6194-6010S_SW_24_06_14

Single-Button Operation

In the case of a two-way or central circuit, the push-button function is also controlled via another sensor. With single-button operation, it is possible to adjust to the current state. To do this, the last value sent has to be loaded to the push-button. For switch objects (1 bit), this involves the values 1 and 0.

In the case of toggling with switch actuators, you can use the status feedback function of the switch actuator.

Also connect the group address of the status feedback object for the connected channel to the switch object (1 bit) for the button function.

Loading values is possible for all object types. Set the same values for all push-buttons, e.g. 70 % for value 1 and 0 % for value 2. If the last sent or received value is the same as value 1, value 2 is sent the after the next action, otherwise value 1 is sent.

For a two-way circuit, check that the objects for the 2 push-buttons are linked to the same group address.

In the case of a central push-button, also connect the central group address to the objects of the other push-buttons.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?