MEG6194-6010S_SW_24_06_14

Off Delay Status Indication

This parameter sets the time for the status indication and screen backlight to be turned off.

Extended settings

Off delay status indication = basis x factor

 
 

Basis

0,1 s/1 s/1 min

 

Factor

5 – 255

When there is proximity sensing, the status is indicated according to the current object value or operation. After leaving, the status indication and screen backlight turn off as soon as the delay time elapses.

When the screen is off, the object value can be updated through the bus, but no indication is given.

During standby, if you select the Unchange option (see Display Settings), the icon status will be updated.

If there is a standby mode:

The proximity sensor cannot directly enter the normal mode from the off-screen state (you need to configure it according to the standby mode).

If there is no standby mode:

The proximity sensing can make the screen go from off to normal mode.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?