MEG6194-6010S_SW_24_06_14

Toggle

With the Toggle function, you switch On and Off alternately with 1 button. This involves single-button operation. You can change and extend the Toggle with the following functions:

  • Send simultaneously with 2 objects

  • Switch on and off and send values

  • Trigger the status indication

Function X – Toggle

...Toggle

Express settings for toggle

 

Name of the channel

12 bytes allowed

Locking function

Disable

Locking = 1/Unlocking = 0

Locking = 0/Unlocking = 1

   

Behavior indication when locking

No

Display lock icon

   

How the status indication is triggered

Switch/value object A/B = On/Off

Status feedback object 1 bit

Status feedback object value 1 byte

Operation = On/Release = Off

Operation = Off/Release = On

Always on = Off

Always on = On

   

Extended settings for toggle

enable

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?