MEG6194-6010S_SW_24_06_14

Programming Mode

You can activate the programming mode in two ways:

  • Press the KNX programming button on the back side of the device.

  • Press one button at the front on each side at the same time as if you want to start cleaning mode and add an extra 5 seconds (10 s + 5 s = 15 s).

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?