MEG6194-6010S_SW_24_06_14

Extended Settings for Toggle

You can select 2 objects. You can specify the object type of each object.

With the 1-bit object type, you can switch On and Off alternately with each button action. The current object value is inverted and then sent to the bus. The values 1 and 0 are sent alternately.

With the 1-byte object type, you can send 2 values alternately with each button action. You can select the values to be absolute (0 – 255) or a percentage.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?