MEG6194-6010S_SW_24_06_14

Principle of the Normal Edge Function

The following diagrams show how the edge function behaves when a button is pressed and released.

Operate button
Release button
Object A Sends telegrams
Sends 1/None Action on operation/action on release

Example 1:

Object A = 1 bit

Example 2:

Object A = 1 bit

Example 3:

Object A = 1 bit

Example 4:

Object A = 1 byte continuously 0 – 255

Value 1 = 255

Value 2 = 50

Example 5: Deadman control/Toggle priority control

Object A = 2 bit (priority control)

Value 1 = 11 (switch on with priority)

Value 2 = 10 (switch off with priority)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?