MEG6194-6010S_SW_24_06_14

Threshold Comparator

Threshold comparator compares the input value with the threshold.

1st Logic

Function of channel

Threshold comparator

Threshold value data type

4 bit, 1/2/4 byte

 

Threshold value

0 – 255

   

If Object value < Threshold value

Do not send telegram/Send value 1/0

   

If Object value = Threshold value

   

If Object value != Threshold value

   

If Object value > Threshold value

   

If Object value ≤ Threshold value

   

If Object value ≥ Threshold value

You can set a threshold, select its comparison type and choose which value to send after comparison:

  • 0

  • 1

  • Do not send telegram

Output send when option allows you to set whether the output should be sent after receiving a new telegram at the input or at every change of the output object.

This setting is wise if a rapid response is expected. It also helps to prevent bus overload.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?