MEG6194-6010S_SW_24_06_14

Text and/or Icons

If you choose to display text or icons, in the next step, you select the desired icon from the menu and enter text with a maximum length of 10 characters.

You can set up to four lines, and the text length depends on the width of the letters. Please verify the correct visualization on the display.

If you select the dimming icon you can also tick the dimming level.

If you tick the dimming level, you then need to set the Stay time parameter. It is the time interval to receive the dimming value from the bus via the Brightness level status feedback object. If the value is received, the dimming level displays in the middle field for the set time. After the time expires, the dimming icon displays.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?