MEG6194-6010S_SW_24_06_14

Extended Settings for Switching

You can select 2 objects. You can specify the object type of each object (1 bit or 1 byte.

The 1 bit object type is used for normal switching.

You can use the 1 byte object type to send a value. You can select the value to be absolute (0 – 255) or a percentage.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?