MEG6194-6010S_SW_24_06_14

Edges with 2 Byte Values

With 2 Byte Edge function, you can send a 2 byte object in floating point format or in integer format (with or without sign). In the default setting, you send the value "10" in floating point format on operation.

You can choose between the normal and extended edge functions and set the following functions.

  • Send values in floating-point format

  • Send values in integer format with or without sign

  • Values per object

  • Action on operation and on release

  • Actions for long and short operation (extended edge function)

  • Send cyclically and with delay (extended edge function)

  • Trigger status indication

Function X – Edges

Edges 2-byte

Express settings for edges 2-byte

 

Name of the channel

12 bytes allowed

Locking function

Disable

Locking = 1/Unlocking = 0

Locking = 0/Unlocking = 1

   

Behavior indication when locking

No

Display lock icon

   

Action on operation

Send value 1

Send value 2

Sends its value

None

   

Action on release

   

How the status indication is triggered

Status feedback object 1 bit

Status feedback object 1 byte

Operation = On/Release = Off

Operation = Off/Release = On

Always on = Off

Always on = On

   

Extended settings for edges 2 byte

 

There is an additional tab under the function tab for setting the 2-byte values.

Edges 2-byte

Edges values

Type of object

Floating point

Integer with sign (- 32768…32767)

Integer without sign (0 – 65535)

[Floating point]

Basis 1/2 (possible values in brackets)

0,01...32768

 

Factor 1/2 (0-2047)

0 – 20,47

 

[Integer with sign]

Value 1/2 (-32768...32767)

- 32768...32767

 

[Integer without sign]

Value 1/2 (0-65535)

0 – 65535

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?