MEG6194-6010S_SW_24_06_14

Button Function

Depending on the type of device, you have a certain number of buttons (2 – 8). You can assign a function to each button.

General settings

Button function

 

Function 1 – 8

No function

Toggle

Switch

Dimming

Blind

Edges 1-bit, 2-bit (Priority), 4-bit, 1-byte values

Edges with 2-byte values

8-bit slider

Scene

RGB lighting

Colour temperature control

Temperature decrease

Temperature increase

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?