MEG6194-6010S_SW_24_06_14

Type of Output Object

If the Sensor is involved as a trigger of the Proximity function, proximity and no proximity states control the Proximity output object.

The proximity output can be set as:

  • 1-bit object - sends values 1 and 0 (no proximity)

  • 1-byte object - sends an adjustable value and 0 (no proximity)

Proximity

Type of output object

No object

   

1 bit

   

1 byte

You can set sending the output values cyclically.

After the device is powered up for one cycle, the output object starts to send the current output value cyclically.

Cyclical sending and sending changes are independent and do not interfere with each other.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?