MEG6194-6010S_SW_24_06_14

Two-Button Dimming

The settings for single-button and two-button operation are largely similar.

For dimming with dimming steps, you can use the parameter Send stop telegram after release.

In the default setting, as with single-button operation, a stop telegram ends the dimming process when the button is released. If, however, no stop telegram is sent, the dimming process continues even after the button is released. A long button action is then enough to dim a step brighter or darker.

If you select the dimming step 1/4 brighter, you can dim from minimum to maximum brightness with 4 long button actions.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?