MEG6194-6010S_SW_24_06_14

Temperature and Text

If you choose to display the temperature, you can select the type of sensor, set the measurement interval, and the time to return from the setpoint to the current temperature.

General settings

Middle field display

 

Temperature only

Temperature + Text

Actual temperature from

Internal/External

 

(Temperature + text)

Description of setpoint

Max. 10 characters

   

(Temperature + text)

Description of internal/external sensor

Max. 10 characters

   

(External sensor)

Interval time of external sensor

1 – 255, unit = 1 min

     

Return time from setpoint to actual temperature

0,5 – 10 s

     

Control mode

Heating

Cooling

Heating and Cooling

If you select the Temperature only or Temperature + Text in combination with setpoint adjustment function (see more in Temperature Decrease/Increase), the setpoint temperature displays when you push the button. After a release, the actual temperature displays after a preset interval. The actual temperature comes from internal sensor or external sensor via bus. If you select the external sensor, you have to set the interval of sending the temperature value request in the next step. If the device do not get the value in the interval time, the middle field display shows ‘’--°C’’.

The display color of the setpoint temperature can additionally be changed by the heating or cooling mode.

The control mode is 1-bit information. If you select Heating, the display color changes to red. With Cooling, the color is blue. If you select Heating and Cooling, the color linked with the Heating and cooling mode object automatically change over according to the value from the bus.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?