Edges 1 bit, 2 bit (priority), 4 bit, 1 byte
The Edge function for 1 bit, 2 bit, 4 bit and 1 byte has a wide range of adjustment options for a variety of individual applications. In the default setting, you switch on 1 consumer when you operate the button and switch it off when you release the button.
You can choose between the normal and extended edge functions and set the following functions.
-
Send with 2 objects
-
Type per object: 1 bit, 2 bit (priority control commands), 4 bit (dimming commands), 1 byte (0 – 100 %) or (0 – 255)
-
Values per object
-
Action on operation and on release
-
Additionally, actions for long and short operation (extended edge function)
-
Additionally, send cyclically and with delay (extended edge function)
-
Trigger status indication
A list of applications with the edge function is provided in chapter Application Examples for Edge Function.