MEG6194-6010S_SW_24_06_14

Blind

With the Blind function, you can raise and lower a blind and adjust the slats.

In the default setting, you raise a blind and adjust the slats. To lower the blind, you need a second button function. You can choose from the following operation concepts.

  • Raise and lower the blind alternately and adjust the slats with each button (single-button blind operation).

  • Only raise or only lower the blind and adjust the slats with each button (two-button blind operation).

  • Move the blind to a previously specified position and adjust the slats.

  • Move the blind back and forth between 2 previously specified positions and adjust the blinds.

Function X – Blind

...Blind

Express settings for blind

 

Name of the channel

12 bytes allowed

Locking function

Disable

Locking = 1/Unlocking = 0

Locking = 0/Unlocking = 1

   

Behavior indication when locking

No

Display lock icon

   

Movement direction of blind

Moving up/down

   

How the status indication is triggered

Status feedback object 1 bit

Status feedback object value 1 byte

Operation = On/Release = Off

Operation = Off/Release = On

Long operation = On/Release = Off

Always on = Off

Always on = On

   

Extended settings for blind

Enable

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?