Proximity Function
If you come within 12 cm of the device, the Proximity function triggers. The display switches on and switches off again after off delay elapses.
The Proximity function is activated by default. You can adjust the proximity triggering (default: built-in proximity sensor):
|
Extended settings |
How the Proximity function is triggered |
Never Proximity object Sensor Sensor or Proximity object |
Value: Never
The function is deactivated.
The display is not affected.
Value: Proximity object
The proximity function is triggered via the 1-bit Proximity input object.
The proximity object has the same function as the internal proximity sensor.
-
1 telegram activates the proximity state.
-
0 telegram activates the no proximity state.
Value: Sensor
The proximity function is triggered via the internal proximity sensor. The internal sensor sends a 1-bit or 1-byte signal to the bus.
The proximity and no proximity states control the status indication.
Value: Sensor or Proximity object
The proximity function is triggered via the internal sensor or the external input object.
The sensor and the proximity object are linked to each other. The result of the link corresponds to an OR link.
If the proximity sensor detects no proximity, it sends a 0 telegram to the bus.
Example:
1 presence detector
The illuminated status indications make it easier to find the push-button and its functions more quickly. You can use a presence detector to control the status indication via the proximity object. If a person is present, the status indication switches on. After the person leaves the room and the preset off delay time has elapsed, the display switches off.