MEG6194-6010S_SW_24_06_14

Switching

With the Switching function, you switch only either On or Off with 1 button. This is a two-button operation.

You can change and extend the Switching with the following functions:

  • Send simultaneously with 2 objects

  • Switch On and send a value

  • Switch Off and send a value

  • Send 2 values

  • Trigger status indication

Function X – Switch

...Switch

Express settings for switching

 

Name of the channel

12 bytes allowed

Locking function

Disable

Locking = 1/Unlocking = 0

Locking = 0/Unlocking = 1

   

Behavior indication when locking

No

Display lock icon

   

How the status indication is triggered

Switch/value object A/B = On/Off

Status feedback object 1 bit

Status feedback object value 1 byte

Operation = On/Release = Off

Operation = Off/Release = On

Always on = Off

Always on = On

   

Extended settings for switching

Enable

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?