MEG6194-6010S_SW_24_06_14

Extended Settings

In the Extended settings tab you can set other device parameters such as:

  • Startup delay

  • Live signal sending

  • Night mode

  • Cleaning mode

  • Language

  • Display backlight level

  • Standby delay

  • Orientation indicator

  • Proximity function

  • Internal temperature sensor

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?