Add Conditions – If
Add a condition that triggers your automation.
There are three types of conditions:
|
Device status change or action |
Examples:
|
|
|
The specific time of the day If you want to define a specific time when the actions take place.
NOTE: Sunset and sunrise-based automations
use the location data from the controller. There may be a slight time
difference between the sunrise and sunset times shown in the app (as
those are taken using different algorithms from the online service
provider).
|
Sunrise |
|
|
Sunset |
|
|
|
Custom |
Define the specific time of the day (hh: mm) and select days of the week. | |
|
Weather changes |
You can define a weather type as a trigger. |
|
|
Energy device value change Depending on the device, you can select different triggers. |
Current power |
See more here: Mapping Energy Data to Energy Groups. |
|
Battery used |
|
You set the If condition for starting the automation as follows:
-
In the automation creator, tap If > tap Add condition and select the trigger to activate your automation:
-
Device status change > select your device and set up its status > tap Set.
-
Specific time of day > choose a start time and repeat period > tap Next.
-
-
Select the conditions under which the automation realizes:
-
Only if ALL conditions are met: Tick All conditions.
-
If ANY condition is met: Tick Any condition.
NOTE: You can add several conditions. We recommend up to 20. -
-
In the next step, select a period when the conditions apply.